The Harmonic Drive® Strain Wave Gear is made up of three basic components. These are first the Wave Generator, an elliptical steel disc that forms the heart of the gear unit, which has a centric hub and a special thin, elliptically deformable ball bearing. The Wave Generator is also connected to the motor shaft. Secondly, the Wave Generator is inserted into the Flexspline – a flexible cylinder with teeth cut around its outer circumference. The Circular Spline surrounds both the Wave Generator and the Flexspline as a rigid solid steel ring with internally cut teeth. What is significant is the number of teeth – the outer toothing of the Flexspline has fewer teeth than the inner toothing of the circular spline. The difference in number is frequently two.